Hi,
I have a design undergoing FCC testing that uses the bq24295 for battery charging / power management. Functionality is fine and we based our circuit off of the reference / application circuits provided by TI. We are using a 2900 mAh li-po battery but using the default charge settings (1A bulk charge current). The charge source is a switching wall-adapter power supply rated for 5V / 3A output with USB-C plug type.
We are failing the radiated emissions test due to noise that is being emitted only when the charge source is connected. The frequency of the noise is about 1.4 MHz. Based on this, it seems very likely that the noise is connected to the charge control circuit.
Has anyone seen this type of problem before? I'd be grateful for any suggestions regarding how to zero in more specifically on the the noise pathway and/or directions to explore for potential solutions. Thanks in advance for any advice,
Brian