Other Parts Discussed in Thread: BQSTUDIO
I used bq34z100 and bq34z100-G, EV2300 and bqstudio to configure it. The following problems occurred:
1、BQ34z100 instantaneous current shows current-41mA in bqstudio. There is only average current in the register settings. I want to read or calculate the instantaneous current from the register instead of referring to the value in bqstudio. What should I do?
2、BQ34z100 shows that the state of charge 24% does not match the full charge capacity and remaining capacity. 24% is incorrect ,Why?
3、Bq34z100-G instead of bq34z100, bq34z100-G 12019.04.23.gg.csv is my configuration file, the voltage should be 13V.SOC and voltage is incorrect。why?