This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM84824: is made using which TI IC . Can I know the part number?

Part Number: TPSM84824
Other Parts Discussed in Thread: ADC12DJ3200, , DAC38RF80, TIDA-01027, TPS54824, TPSM84424, TPSM84624

Hi ,

We have selected TPSM84824 series to used with ADC12DJ3200 and DAC38RF80 as used in TI reference design TIDA-01027.

But I want to know the part number of ICs with which these power modules are made?

Thanks,

Lalit

  • Hi Lalit,

    The internal IC of the TPSM84824 power module is the TPS54824 SWIFT step down converter.

    Regards,

    Jimmy 

  • Hi Jimmy,
    Thanks for the info.
    Can u please also tell me the part number of the ICs used in TPSM84424 and TPSM84624?
    Also in the datasheets of all three modules , the inductor value gien in the block diagram is 0.85uH.
    Can you please tell me the part number and make of the inductor used in these modules?

    Thanks,
    Lalit
  • Hi Lalit,

    The IC used internal to all 3 devices is the TPS54824. The internal inductor is a custom part number designed for these devices. Is there some specific spec you are looking for?

    Thanks, Jason

  • Hi Lalit,

    Since we have not heard back from you for some time, I'd assume that your issue has been resolved on your end. Because of this I will be closing this thread now. If you have any further questions I'd recommend creating a new E2E post and an application engineer with get to it in a timely manner. Thank you.

    Regards,
    Jimmy