Other Parts Discussed in Thread: TPS22917, TPS22916, TPS22919
Hi team,
The application power path is CR2032(3V battery) --> TPS22960(there is another button switch between CR2032 and TPS22960 ON pin) --> MCU
Due to the mechanical design, need a part max height< 0.7mm and no ball lead package. I didn't find any single channel part meet the requirement and just the TPS22960 meet the requirement. We connect Vin together, VOUT together, ON together and used as single channel.
It's with battery power system, total current should be very very small for longer life time.
In datasheet, ON pin cannot let floating, we will let ON pin with a pull down resister and connect to MCU GPIO.
We would like to know ON pin pull down resister can be 3Mohm for very small power dissipation?
Or do you have any recommend single channel part meet the requirement?
Thank you!