This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51200: Behavior when REFIN is over 1.8V

Genius 17335 points
Part Number: TPS51200

Hello,

 

My customer has an question about TPS51200.

They want to input 1.8V to REFIN input pin.

But since the recommended operating range is up to 1.8V, there is basically no margin for 1.8v REFIN input.

What kind of problem could occur if REFIN input is over 1.8V.

 

They understand we can’t guarantee any operation if the recommended operating range is not kept.

But what they want to confirm is whether this device could have something very strange of non-linear behavior.

 

Regards,

Oba