This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28019A: Whether UCC28019A support the DC input

Part Number: UCC28019A

Hi Expert,

The customer is asking whether UCC28019A can support the DC input design.

Conditions:

--The input is 200Vdc~400Vdc

--Output is 410V with 2.6A

Best regards,

Eric Lai

  

Field Application Engineer

Texas Instruments Taiwan Limited

O: +886-2-2175-2582

M: +886-909-262-582

E-Mail:Eric.Lai@ti.com