Other Parts Discussed in Thread: TPS562200, , TPS62147, TPS62148
Hi
We are evaluating TPS62150EVM-505 and facing problem of unwanted radiation noise.
Measured noise is attached in following file.
Input : 9V
Output : 3.3V/0.4A
You can see radiation noise at 300MHz -400MHz with TPS62150EVM.
As comparison, measurement result of TPS562200 is also attached.
Radiation noise was not observed with TPS562200.
Why is the radiation noise occurred with TPS62150EVM?
Could you please tell me how to avoid or suppress radiation noise?
BestRegards