I am using a bq34z100-G1 and I created a “golden image” / configuration for my battery that I load into the gas gauge. After I load my configuration / golden image I can confirm it starts out with the impedance track disabled.
What I do is the following:
Step 1) flast the firmware in the bq34z100-G1
Step 2) now load my settings into the bq34z100-G1 .
Step 3) verify RUP_DIS=0 and VOK=0
I am following the flowchart on page 54 of the Ref guide linked here after I configure the bq34z100-G1 for my battery by applying the golden image to the bq34z100-G1:
http://www.ti.com/lit/ug/sluubw5/sluubw5.pdf
The first part of the flowchart shows I should start out with the gas gauge showing RUP_DIS=0 but my device starts out with RUP_DIS=1. I can confirm that VOK=0.
What settings should I check as to why after I first apply my settings / golden image I would start out with RUP_DIS set to “1” and not "0"?
Thanks,
Doug