This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2421-2: Current consumption

Part Number: TPS2421-2
Other Parts Discussed in Thread: TPS22810, TPS25200, TPS2595

Hi,

In datasheet table, VIN Bias current at /EN=0 is typ 3.9mA.

Does it means that TPS2421-2 consume the 3.9mA current during operation?

Customer needs the device which has total current consumption below 100uA.

Could you recommend proper device?

Condition is as below.

input voltage: 4V~9V

Current: 2A

operating current consumption: below 100uA

short protection is mandatory.

Customer evaluated TPS22810 but when it is under output short during long time, device is damaged.

Thanks.