Part Number: BQ25601
Other Parts Discussed in Thread: BQ25606, , BQ25895
Hi team,
Could you please let me know the recommended part# for below use-case ?
- Input: DC12V
- Output: 9V, 7V, 6V, 5V, max.3A
- Battery: 15Ah LIB1 battery, 4.2V charging/dis-charging, Full charge in 2.5h or 5h.
- Power supply path: Red in below.
- Want to change the output voltage by the external resistor via MCU
It would be grateful if you could provide your recommendation to me as soon as possible, thank you.
Regards,
Jun