Hello Everyone,
I am using the BQ24170 for designing a 2S Lipo charger. Now, while designing from the reference circuit diagram, I am unsure about the battery connection to the output (VBAT).
I am not sure whether I should keep a provision to connect the Battery's Charge/Discharge leads (to VBAT) or if I should keep a provision to connect the 'Balance charging port' to the VBAT output or if I should do both.
Can you suggest the relevant circuit diagram for the output connection (VBAT) with the battery?