This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2359: Set 3.3 V rail output current limit to 250mA

Part Number: TPS2359

Hi all,

Both channels of TPS2359 are used. One channel uses 3.32K, which still follows the AMC requirements, and the other channel uses 2.3K to adjust the current limiting point, nearly 250mA is needed. By adjusting RSUM3X to 2.3K, 283mA overcurrent point is set. No other modifications are made; the schematic diagram is as follows:

As the max continus current is not specified, I want to know if 250mA continues current is  allowed for TPS2539. The enviroment temp is about 75 degree.