Hello
I want to connect two leds in serial connection to each output of this driver. In all documents I see one led to each output and anode of it connected to 5volts. Is it correct con connect two leds in serial and power the string to 12 volts (VLED, anode of the 1st led of the string = 12V)?
The leds I want to use have a 3v drop Vf at 30mA current
thank you for your prompt answer