This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24195: Using USB D+/D- simultaneously for USB-Charger-Detection & USB-UART-Bridge

Part Number: BQ24195


Hi Team,

my customer is plannig to use the BQ24195 in one of their designs. The Application requires a USB-UART-Bridge, ideally using the same USB-Port as the Charger.

Question:

is it possible to use the D+/D- lines of the USB connection simultaneously for BQ24195's USB-Charger-Detection and a USB-UART-Bridge?

- Given that: The reset of the USB-UART-Bridge will be on hold as long until the BQ24195's USB-Charger-Detection is completed.

Can you help us out here - thank you very much!

Kind regards

Dierk Bronner