This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51200: Input and Output Capacitance

Part Number: TPS51200


Hello,

The datasheet for the TPS51200 part recommends using 1/2 of the output capacitance on the input. Our current design has about 30uF capacitance right at the output of the converter and about an extra 400uF local to the DDR4 memory. I was planning to put about 20uF on the input but am wondering if I need closer to 0.5*430uF = 215uF on the input as the datasheet recommends. Can you please confirm if the 20uF is sufficient or if I should target closer to 215uF. 

Thanks!

Matt