Other Parts Discussed in Thread: TPS61170
Hi all,
In our design, we are using the TPS61170 to convert 12V input voltage to 27V. The feedback is controlled by a PWM signal that is used to ramp up the output voltage(to limit the inrush current to the high output capacitance)
Due to a high output capacitance(and ESR) on the output, I need to add a small capacitor in the compensation circuit.
We also want to improve the bandwidth of the system, we want to recalculate the compensation resistor and capacitor.
For this, we are using SLVA913C application report of this boost converter.
In the Se formula(I think this is for the Slope compensation ramp), there are 3 variables mentioned where I can't find a value for; A F and D.
I also have another question; this added capacitor, how can this be implemented in the transfer function Gt(s)?
Can you please help me to find these variables?
Thanks,
Stijn