This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2596: Dual output LM2596

Part Number: LM2596


Hello community good afternoon

Need to implement a solution that outputs 5V (1.5 Amps) & 12V (2.5 Amps) from an input voltage of 12V or 24V.

Is there any LM2596 or similar with dual output?

Thanks!