This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: Bq4050 shutdown

Part Number: BQ4050

Can you please  explain the use of shutdown mode if entered via the ManufacturerAccess() MAC Shutdown command.  Since the FET's are turned OFF, if I issue the shutdown command while VCC is (say) 12V, the device can only be awoken once a charger is attached ( "when the voltage at the PACK pin > VSTARTUP")?

Thanks