Other Parts Discussed in Thread: BQ78350, BQSTUDIO, EV2400
Tool/software: Code Composer Studio
Greetings,
I have a new custom board with a BQ78350-R1 device connected to a pack with Samsung INR18650-30Q batteries. I need to update the chemistry in the BQ chip. However, I get "Error code = 1253" and a red error status at the bottom "Chemistry programming Error: Client waited more than 30 seconds for pipe."
Any clues as to what the issue could be?
Security mode bits (SEC1, SEC0) are set for Unsealed.
Otherwise I can talk to the BQ78350 with no issues other than my capacity says it's at 3% when my average cell voltage is 3.4Volts.
Thanks,
Gary