Other Parts Discussed in Thread: TPS61199
Hello
I want to check the PWM Duty range, I find in datasheet,it recommend min PWM Ton is 10uS, so for 20KHz PWM, it min Duty is 20%,is it right?
I find TPS61199 's recommend min PWM ton is 1us, so it min Duty is 2% for 20KHz.
What's factor to limit this min pwm Ton ? one competitor's PWM duty range could be 1%-100% in range of 100Hz-20kHz.such as RT8532