Requirements +5Vin, -15Vout @ 0.3A
Circuit designed from Webench using these specs. When prototyped, it does not regulate well above 150mA. Even at this modest load, inductor gets hot but -15V is present. Above 150mA, regulation is lost and droops to around -8V. Also this regulator would not start up into a very light load (20mA) without a 22n capacitor connected to the SS pin.