Hi,
I am working on project where I need to do AC to AC conversion, requirement is mentioned below.
Input supply: 110VAC 50Hz frequency
Output Requirement: 230VAC 60Hz frequency/ Output load current 10A
I can see two option for this as mentioned below.
1. Cycloconverter
2. DC link converter (AC to DC and DC to AC)
I am confused which topology is better considering the output waveform performance and harmonics. As cycloconverter need less power stages, so size benefit is there in cycloconverter.
Could you help me to get figure out the best topology for above application requirement?
Also, Do we have parts suggested from TI for this kind of application?
Regards,