Other Parts Discussed in Thread: BQ76PL455A, EMB1499Q
Hi there, we are manufacturer of Low Voltage 48V 16s LiFePo4 Energy Storage solutions and currently developing replacement of our old Bms (MAX14921 with passive balancing) to active balancing, What is the easiest conversion from the existing design of EM1402EVM to work in single BMS board mode and capable of moving energy from pack to cell and cell to pack. Also is it possible to use EM1402EVM without 12 battery in stack with 2 or more BMS to transfer cell to 12 and 12 to cell (PACK(n) cell (m) to PACK(o) cell(p))?