can we power the system and the battery with different voltage? how?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Belhaj,
You can power the system at a higher voltage than the battery is being charged with, but the system voltage is never below the battery voltage.
Having a higher system voltage than battery charge voltage will happen automatically if the MinSystemVoltage register is set to a value higher than the battery voltage. Note that in this condition, the BATFET will be driven in LDO mode (in order to generate the appropriate lower voltage for charging the battery), which will be less efficient charging than when MinSystemVoltage is below the battery voltage and the BATET is fully enabled and the battery is being charged directly from the output of the switching regulator.
Regards,
Steve