Other Parts Discussed in Thread: TPS2121, TPS22917, TPS22916, LM66100
Hi Gurus!
I'm considering using the TPS22990 as a switch to select between to power supply outputs to a common rail. My question is, is the device back-feedable? For example, if there is a voltage on the output while there is no voltage on the input, will the output voltage run through the body diode of the FET show in the function block diagram, page 16 of http://www.ti.com/lit/ds/symlink/tps22990.pdf ?
Then, how do I make sure I am not ordering the part with the option discharge path?
Thanks so much for your insights!
Keith.