This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23754: Reference design or EVM for PoE+ and 1000base-T solution

Guru 19685 points

Part Number: TPS23754

Is there Reference design or EVM for PoE+ with 1000base-T solution?

I looked like existing PoE+ designs are 100base-T only.

(For example, TPS23754's EVM, etc) 

If there matched design: PoE+ with 1000base-T the other than TPS23754, it is OK.

Best regards,

Satoshi