This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Calibrating the BQ34Z100-G1 CC Offset and Board offset

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQSTUDIO, BQ34110

Is there any documentation that describes the steps to calibrate the BQ34Z100-G1 via the I2C commands?

For example, if I want to calibrate the CC Offset and Board offset via I2C.

I assume I would be using the commands to calibrate the  CC Offset and Board offset.

CC_OFFSET  0x000A

CC_OFFSET_SAVE  0x000B

CAL_ENABLE  0x002D

EXIT_CAL  0x008D

ENTER_CAL  0x0081

What are the steps to calibrate the CC Offset and Board offset?  Is there anything that needs to be polled during the calibration process to verify the calibration is complete before the data is saved?

Doug