I have two questions related to creating a golden image after the gas gauge has been configured and been through the process to learn the battery and achieve an update status of 6.
Question 1: The documents I have found on the process to create the golden image say to change the update status from 6 to 2 as one of the steps to create the golden image. Are there any steps that need to be taken after the golden image is programmed on a new device / system before the Impedance Tack is re enabled? If there are no special steps required, why would it be necessary to set the update status to 2?
Question 2: If there a list of other parameters that should be reset when the cycle count is reset? I assume anything that says lifetime or any lifetime data would need to be reset.
Thanks,
Doug