This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24297: Customer needs info on RBFET ,when in off state, current is being pulled thru the diode, from VBUS to PMID

Part Number: BQ24297


Hi Support team

My customer is using the BQ24297 in a very nonstandard ckt. In one of the modes they will be pulling current thru the RBFET(Q1) parasitic diode (fet is in offstate). This current can be up to 500mA and the ambient temp may hit 65C. Does this present a thermal issue for the part? Can this damage teh part or cause it to lock up or improper operation?

Thanks

Jeff Coletti

  • Hi Jeff,

    In general, the parasitic body diode can handle the same current as the FET when it is on. However, we have not tested this particular configuration over temperature so I cannot warranty the operation.

    Regards,
    Jeff