This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: Data memory can not be rewritten.

Part Number: BQ34110
Other Parts Discussed in Thread: BQSTUDIO
environment  
win10
bqstudio V1.3.86 
bq3410FirmwareBundle 0.02
Divice 010.0.02
FULL ACCESS 
The bits of SEC1 and SEC0 are 0.1
Rewriting response  A read data write failed comparison
Is something wrong?
  • The most likely reason is because the parameter "Flash Update Ok Voltage" is set higher than the voltage observed at the BAT pin of the device. If you follow the steps in Section 3.2.1 of the EVM User Guide, you should be able to update this parameter so that you can write to the data flash.

    Best regards,
    Matt