This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9248: Data Flash and Program Flash in UCD9248

Part Number: UCD9248

Is my following understanding correct?

Data Flash and Program Flash exist in UCD9248. User can download firmware to data flash but not to Program Flash.  User firmware is only composed of data. The program is downloaded by TI and can not be modified. Checksum is used to start the program on power up. If checksum is correct, UCD9248 runs the program. If not,  UCD9248 wait a command to execute program.

Thank you

  • Hello,

    Data Flash and Program Flash exist in UCD9248. User can download firmware to data flash but not to Program Flash. User firmware is only composed of data.
    Q: Yes.

    The program is downloaded by TI and can not be modified. Checksum is used to start the program on power up. If checksum is correct, UCD9248 runs the program. If not, UCD9248 wait a command to execute program.
    Q: What program do you refer to, TI Fusion?

    Thanks
    Qian
  • by "this program", I mean the content in program flash, not the fusion software.
    Thank you.