This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5020: 80V DC to 160V DC Boost Regulator - Reg

Part Number: LM5020
Other Parts Discussed in Thread: UCC28780

Dear all,

We are proposing to use LM5020 IC to convert from 80V DC to 160V DC.

Output current is around 9 Amp.

With the reference circuit of PMP10523 as base, whether it is possible to increase the Power Path components such as MOSFET,

Inductor and Diode rating to around 10Amp and use the same. Any other constraints to be taken care of?  

Link: http://www.ti.com/lit/df/tidrr99/tidrr99.pdf

Thanks in Advance.

With Best Regards,

B.Saravana Vikram.