This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2734: Tolerance

Part Number: LM2734

Hi TI Team,

For the LM2734 Vfb voltage, as you can see, the Vfb reference is from 0.784V to 0.816V If Tj from -40degC to 125degC.  I believe that this tolerance (0.784V ~0.816V) includes initial tolerance and  temperature variation.

For a specific part, for example, if the Vfb is 0.801V at Tj=25degC, what Vfb would be if Tj=-40degC and Tj=125degC ?   Can we refer to the chart shown in Table.2 for Vfb temperature variation? 

Table.2  shows that Vfb changes only 4mV (0.802-0.798V=4mV) variation if Vfb temperature changes from -40degC to 125degC?

The reason we asked this question is that  the initial tolerance (normally in 25degC) can usually be eliminated by calibration, but the for the temperature variation, it can not be calibrated. So we need to know the tolerance caused by the temperature variation.

 

Table.1  LM2734 tolerance

Table.2  Vfb variation vs temperature