This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25085A: Motor drive using SWPS

Guru 16770 points
Part Number: LM25085A

Hi

The customer considers DC motor drive system using LM25085A.

The requirement for LM25085A is as follows.

INPUT:17V-25.2V

OUTPUT : 16.2V/3A (8A peak)

EN function

4276.e2e.xlsx

It does not have motor driver, just applied power to motor directly and rotation is controlled by  EN of LM25085A.

To wait output stable before applying voltage to motor, FET is inserted at Vout.  FET ON/OFF is controlled by MCU.

In addition, to protect the impact of back EMF from motor, diode is inserted prior the motor.

Do you think it is feasible?

Could you please give me your feedback if you had concern?

BestRegards