Other Parts Discussed in Thread: BQ25570
Deal Ti
I am working with BQ25570 EVM-206, setting MPP = 80% ( Voc_samp = 80%) . Input is a GaAs single crystallize ( Voc = 0.94 V, Isc = 16.04mA) at 16600 lux from LED light and I get the result at VBAT ( VBAT = 4.19 V, IBAT = 5.16mA). So the output power larger than the input power, exceeding 100%. Could Ti give me some explanation about this problem ?
Thanks.
H.Thuc