This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9248: My UCD9248 firmware project debugging

Part Number: UCD9248

I have two versions of UCD9248 firmware projects. Both of them have bugs. I hope you can tell me where the bug is.

This temp_import_error_and_clf.zipis the first firmware project. Firstly error occurs during importing. Secondly, after importing (I disregard the import errors and go on), CLF error occurs when I turn on the PWM during monitoring.

This temp with spark.zip is the second firmware project, spark occurs when I turn on the PWM when monitoring, because over voltage fault limit is reached and PWM is turned off. If I set PWM do not turned off, the voltage will be stable at a value obviously larger than my setting.

Thank you.