Other Parts Discussed in Thread: UCC2804
Hi Experts:
customer designed the flyback with the two isolated output by UC2844. One is 15V for the UC2844 power supply and the another is 24V for the system power,
The feedback is on the 24V rail.
When shorting the 24V, the UC2844 will enter the cycle by cycle current limiting mode constantly , it will make the Mosfet damaging because the chip has no hiccup mode which will latch the driver for a long time. So customer has to change the design due to this issue .
Could you please recommend a new chip with the hiccup mode or the aux winding voltage monitor to protect the over current case, and should only change a little in the current design ?
Thanks!