This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25890EVM-664: BQ25890HRTWR

Part Number: BQ25890EVM-664

Hi

I have a problem with BQ25890EVM-664 evaluation kit, VIN I connect it to 5V, when I connect the battery in BAT and it has a charge of 3.3V-3.9V this voltage is observed in the SYSTEM. When I do not have the battery connected in both BAT and SYSTEM pins I have 4.2v.


I need that always in SYSTEM there 4.2V and that the battery is charged, I also need a current of 5 A

What can I do to get this?


In other projects I have used this component BQ24076RGTT but it is 1.5 A, I made the change to have more current (5 A), but I want it to work like this BQ24076RGTT.

I am looking forward to your response.
 

Thanks.