This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50: how to limit charge current

Part Number: BQ40Z50
Other Parts Discussed in Thread: BQ40Z60, BQ24610

We design a BQ40Z50 board to support a 3.35A pack (4 cells).

Set of registers seems to be correct following guide R3

Charge and discharge works.

But there is a subject that surprise me.

As we have set registers to do a charge at 1650mA @ 4v2 max, we see that the current goes up to 1950mA.

And more precisely, if we increase the current capability deliver by the PS, the current charge varie with the current deliver by the PS.

Sure that we miss something but where !!

Regards

Gilles