This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65917-Q1: Where can I find each OTP revision power sequence setting.

Part Number: TPS65917-Q1
Other Parts Discussed in Thread: TPS65094, LP8733-Q1, LP8756-Q1

Hi,

     Customer want to find a PMIC for AMBA CV22/CV25 platform, the competitor are DA9063 and DA9062.

I suggest they choose TPS65197-Q1 ,but in other e2e thread mentioned  the power sequence can't modify through i2c/spi by MCU.

So I want to know how can I found power sequence plot of each OTP revision , I didn't found in datasheet. Is it just for TI  platform like TDA/DRA/?

Or could you suggest me another PMIC part number ?

Customer need 4 channel buck (one of the four channel need 0.75V/5A rating, another  less then 1A) and 4 channel ldo.

Thanks