Other Parts Discussed in Thread: BQSTUDIO
I am trying to reprogram the ChemID of bq27541 using bqtool SDK, but I can't figure out how to use either of these commands:
For the below ProgChem command, it returns the following error:
"Function failed. Error code 1422. Translated Requested data not found."
It is due to the chemID I entered does not exist?
If so, which directory should I place the "chemistry" folder or files?
int ProgChem | ( | const char * | bqzContainerName, |
const char * | commandpipeName, | ||
int | chemID | ||
) |
For the below ProgChemFile command, I cannot figure out the way to extract a single chemistry ID file.
I am assuming this is ".chem" file but is there any way I can generate target ChemID's chemistry file using Battery management studio?
int ProgChemFile | ( | const char * | bqzContainerName, |
const char * | cmdChannelName, | ||
const char * | chemFileName | ||
) |
Thank you for your support.