This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: LM5175 USB typC PD with TPS65987

Part Number: LM5175
Other Parts Discussed in Thread: TPS65987, ,

We are in the process of brining up the board overseas as I write this email so it is critical if you can get back to us asap. We have TPS65987 USB type-C controller programmed in Source/DFP mode. We are following the reference design for TPS65987using LM5175 as source for VBUS connected to PP_HV2 of TPS65987. We has simulated the LM5175 design on Webench and bias is 5V instead of 9V as suggested by Webench simulation. The problem we are seeing is that USB Type-C takes some time to negotiate PD contract and at times it keeps trying but never negotiates the contract.  Even when it does negotiate PD contract it charges the devices connected at very low current like 60 mA – the max it goes upto is like 400 mA.

We have isolated the problem to LM5175  by disconnecting it from the circuit and providing 5V externally from benchtop supply. The system works fine and right away negotiates PD contract and starts charging devices connected at 5V 1.A to 1.2A range.

I can't attach schematic in this forum - PSIL060A(001)_Sch.PDFLM5175_simulation.pdfdifference from simulation results  is  LM5175 is in DCM mode by grounding mode pin. We also have ADCIN1 set to 100K to GND . I am attaching LM5175  Webench simulation and TPS65987 reference design. This is of high urgency as we are overseas and I would appreciate a quick feedback.LM5175_simulation.pdfPSIL060A(001)_Sch.PDF