This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2961: bq2961

Part Number: BQ2961
Other Parts Discussed in Thread: BQ2962

Hi

I would like to have overvoltage 3.8V and under voltage 2.3V, what is the full part number of the BQ2961 device. Its not mentioned in the datasheet.

Can you please advice on this subject.

Thanks and Regards

Dileep Chacko

  • Hi Dileep

    There is a bq2962. Does that not work for you?
    thanks
    Onyx
  • Hi Onyx

    I got the part number from the datasheet BQ296103DSGR, but later I found that, overvoltage protection and under voltage protection as 4.5 and 2.5V respectively. I would like to have 3.85V as overvoltage protection and 2.1V as under voltage protection. My understanding is that in order to get this value I should request TI to make custom made. bq2962 also has the overvoltage protection and under voltage protection as 4.35V and 2.5V, I still need to order custom part from TI. Do I get any standard part which has overvoltage protection and under voltage protection 3.85V and 2.1V respectively. My application is for Lithium Ion battery (LFP). Can you please advice.


    Thanks and Regards

    Dileep Chacko
  • Hi Dileep

    Unfortunately, the answer is no. A request has to come in for that.


    thanks
    Onyx