Part Number: BQ25883
Other Parts Discussed in Thread: BQSTUDIO, BQ25882
Tool/software: Linux
Hi, we are using BQ25883 to charge a Linux/Android device. The Linux driver references a usb_psy power_supply, that it -among other things- uses to set charging current depending the type of the usb supply. I find this a bit confusing. Do I need another part that does the USB charging type handshaking or does the BQ2588x do handshaking with the USB host to determine the charging type (SDP/CDP/DCP)?
We also have the EVM (with BQ25882) and this seems to do the handshaking without another part. but this is Windows, so I have insight into how it is done from within bqstudio. On a sidenote, the bq25882 evm completely stopped working with bqstudio ever since I had the evm hooked up to my Android/Linux board. Cannot reproduce the charging test any longer, it says Not Power Good (while the PG led is on) and No input, while I have a USB cable connected...