This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63060: Single LiPo to 3.3V converter

Part Number: TPS63060
Other Parts Discussed in Thread: TPS63020, TPS63802

Hi

I have to convert from Vbat (from a single cell Lipo battery) to 3.3v @ 1A. The project requires a low quiescent current (say less than 30uA). It looks like the TPS63060 is Texas's best alternative.

Is there any other solution?

BR

Gilberto

  • Hi Gilberto,

    The TPS63060 is more suitable for multi cell batteries. A better alternative is the TPS63802. The quiescent current is well below 30 µA, and for Vout=3.3 V it can support Iout=1 A down to Vin=2 V, whereas the TPS63060 can go down to Vin=2.6 V. However it is still in preview phase, but preproduction samples are available. Otherwise the TPS63020 is also a better alternative, with higher Iq than TPS63802 but lower than TPS63060. Compared to the TPS63060, it can operate at lower input voltages and support 1 A down to Vin=2 V.

    Is there any other requirement, such as extra functions or package type?

    Best regards,
    Milos

  • Hi
    I am trying to avoid BGA package. So, TPS63802 would be a good alternative. Do you have a final number for the quiescent current?
    BR
    Gilberto
  • Hi Gilberto,

    The quiescent current is 11 µA, you can take a look at the electrical specifications in the datasheet. This results in a no-load input current of around 20 µA.

    Best regards,
    Milos

  • Hi Gilberto,

    We haven’t heard back so we're assuming this answers your question. If not, just post a reply below, or create a new thread if the thread has locked due to time-out.

    Thanks and regards,
    Milos