Hi There,
Please see my questions below..
1) Page 3 of the Data sheet says MPPSET pin needs to be set to 1.2 volts through a divide network. How can we guarantee this will be 1.2 volts when the input is a solar panel which will
vary over a voltage range ?
2) Page 3 of the Data sheet says that VREF can be used as a pull up for Pins STAT1 AND STAT 2. This confuses me because I though the pull up for the 2 STAT pins was VIN as labeled in the schematic on page 22. Is the VIN labelled as "Solar Cell Half Panel" the same VIN that's used to pull up stat1 and 2 through R7 and R8 ?
3) Please explain the use of the ground with the down-facing arrow and the chassis ground on page 22. Which ground does the battery connect to and which ground does the solar panel connect to ?
4) I see no explanation for C9 in the schematic on page 22 . Can you explain it's purpose ?
5) Please indicate from the schematic on page 22 which Capacitors are the input and output as referenced in the calculations on page 23 steps 9.2.2.2 and 9.2.2.3.
6) I've noticed that the FETs recommended are of the "PowerPAK" dual package design . Is this imperative for frequency and capacitance specifications ? I was hopping to use 2 descrete D-PAK versions. Are they acceptable for this application ? We will probably not be running at 10 Amps but more likely at 2 amps. Please comment.
Thank you
Dave