Other Parts Discussed in Thread: BQ25100, BQ51003, TIDA-00318
I am designing for a tiny device application which requires a battery in the 240mAh. The charge current will be 200mA. I have seen a number of supprt requests for the low current operation, but I do not see the relevant specification in the datasheet. The BQ51050B is attractive since it eliminates the additional battery charger. Could you clarify what or where are the limitations at these 1W power levels?