Hi support team, could you please give me the following information : the max continuous input (or clamping) current that the circuit withstands on each output when the circuit is supplied or not. Or confirm that the circuit withstands continuous input current up to 20 mA between each output and GND or VDD. The D.S. is not very precise concerning the clamping protection : 'In many cases, the external Schottky diode clamps may be eliminated because the presence of the MOSFET body diodes offers low impedance to switching overshoots and undershoots '. I just need to know if the clamping (or body) diodes are efficient on both GND and VDD supply voltage, on each output, up to 20 mA (or more). Thanks in advance for reply. Cdlt Jean