This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Multiple outpout DC-DC or LDO recommend

input 9Vdc-38Vdc:

output

voltage

current

topology

2 channals

5V

~250mA

buck

3.3V

~100mA

buck

3 channals

5V

~250mA

buck

3.3V

~100mA

buck

15V

1.2-1.5A

buck-boost