Other Parts Discussed in Thread: LM5155
Hallo everyone,
I want to use the LM2587-5.0 as described in Fig.29: “Triple-Output Flyback Regulator” of the manual. My question is: Can I use a 11V input Voltage, if I want to generate two output voltages, one above the input voltage (e.g. 12V) and one below the input voltage (e.g. 5V), although the manual suggest a voltage between 18V to 36V?
For this configuration, I’m using a Transformer T4 (PE-68422), as described in Table 2 of the manual.
Many Thanks
Franz Braun